STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411RE Unable to make UART work.

Hello guys.I've been trying to learn how to program STM32 MCU's using registers.This time, I've attempted to configure a basic UART programm in which I would like to send whatever I receive via UART back to the source. Basically an echo program.I'm i...

IRoja.1 by Associate
  • 2702 Views
  • 4 replies
  • 0 kudos

Resolved! stm32l552 bootstrap

Hi,I have a NUCLEO L552 and I would like to run a very simple program (just blinking a led).I have placed my vector table @ 0x08040000 as described by the data sheet. to program the flash I use the J-Link from Segger. What is strange, is that I canno...

STM32F446 ADC modes for analog watchdog

Hello,I'd like to use my STM32F446 in the following way:ADC 1&2 are connected to an analog sensorOnce the sensor connected to ADC 1 passes a certain voltage, start using DMA to transfer ADC 1&2 values to buffers.Once the transfer is complete, stop th...

RZige.1 by Associate
  • 2105 Views
  • 3 replies
  • 0 kudos

STM32L476RG USART not transmitting?

I'm trying to send exactly 8 bits of data, and check my results with tera terminal, however I'm not seeing anything come up. I noticed that on the block diagram for the STM32L476RG nucleo board, that the APB1 Bus is also connected to AHB1, but there ...

kfg4 by Associate
  • 1366 Views
  • 2 replies
  • 0 kudos

Unable to communicate with LCD2004a via I2C (Nucleo-F103RB)

Hell guys, i'm trying to communicate with LCD2004a with the I2C extender.i followed this guide https://www.youtube.com/watch?v=7mQppaEJjT4what i did:I generated project using CUBEMX to Keil uvisionconfigure I2C with those parameters: 100Khz CLK, slav...

Oyose.1 by Associate
  • 2078 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F746 SPI basic usage

Hi everybody! I've been struggling with this monster for a few days now. I'm trying to make it do some very basic (pun not intended) things and I have little hair left... But let's cut a (too) long story short: I'd like to send with the SPI a few byt...

luch by Associate III
  • 2466 Views
  • 3 replies
  • 1 kudos

Clarification of Entering, Leaving and Remaining in Sleep

Suppose that my system consists of 3 modulesmain... at the end of the while loop, I want the system to enter sleep mode, so at the end of the while, I put wfi(); or possibly I put DSB(); after that. Other examples replace wfi() with HAL_PWR_EnterSLEE...

DRobe.4 by Senior
  • 2695 Views
  • 5 replies
  • 0 kudos