STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Trigger scan mode

I am using stm32h745i-disco.I need to run ADC in ScanConvMode mode because I need the exact sampling frequency.But my ADC constantly gets into HAL_ADC_ErrorCallback with code 2 (Overrun).I noticed that the call frequency of HAL_ADC_ErrorCallback is s...

Can stm32 mcus work with TM1809 led driver?

I'm trying to get TM1809 led driver working with stm32 mcus, I tried with f103 and f030 ones but had same results, I can successfully send 1 to the driver but can't send 0, looking at it with oscilloscope it seems even at low-est delay possible the p...

AJava.5 by Associate
  • 1575 Views
  • 4 replies
  • 0 kudos

STM32F334 use both TIM16 DMA channels

Hi there, I tried the hole day to use two DMA channels (TIM16) as depicted in thereference manual. If I understand it right, there is the option to use channel3 and channel 6. At channel 6 the update event can be disabled. That’s exactlywhat I need, ...

DRH by Associate III
  • 1199 Views
  • 3 replies
  • 0 kudos

hi guys, I've been trying to write to internal flash for the last two weeks, and unfortunately, I didn't manage to do so. I worked with the function I have from the library and read in the manual.

tst= 0x121212121212HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,0x8000000,tst); the address i took from the manual as well. i cant understand whats going on, please help me.thanks a lot

0693W000001cO3YQAU.png
Gbasi.1 by Associate II
  • 6164 Views
  • 18 replies
  • 0 kudos