User Activity

Hello,I know that there are voltage/wait states limits for the FLASH memory. Do they apply also for the EEPROM memory? I don't believe so, also the StdLib function FLASH_SetLatency() doesn't have analogous EEPROM function and etc. Also I didn't find ...
Hello.I'm using STM32L151C8T6 for some simple task. In the beginning I used MSI clock and everything was fine. But I decided to switch to HSI and now I got problems using USART1, namely I think that the USART1 periphery isn't properly initialized due...
Posted on May 26, 2017 at 01:19 Hello. I'm trying to use the RTC Alarm interrupt to execute code at a specific time interval. I did everything, but the interrupt code never gets executed. However, all registers seems to be properly set. Fin...
Posted on March 09, 2017 at 11:01 Hello! I would like to use the ADC with DMA in order to do the following: - manually start the ADC in (discontinuous) scan mode - sample 3 channels - put the adc result with DMA to some array. - no...
Posted on December 28, 2016 at 10:22The original post was too long to process during our migration. Please click on the attachment to read the original post.