User Activity

Hi! When I connect stlink v3 minie , lounch cubeide -> stlink upgrade , it only shows "V3",  nothing more. I can't open it for upgrade.Other embedded in nucleo boards stlink v3 works and can be upgraded (nucleo G431 and H723).There is an error about ...
What is the best way to protect pin from external 'high' voltage (10-30-60 or higher V). Is it even possible without external buffer, resistor + clamping ​diodes etc.?​Input with high Z, open drain, other methd for "disconnecting" pin will do the job...
How to set up white noise in stm32g431kb DAC?​DAC works, I can produce sine wave but cant generate white noise.​​​I set DAC->CR WAVE1 to 01 (noise), DAC->CR TEN1 to 1 (trigger enable) and DAC->CR EN to 1 (enable). Tried to set also DAC->CR MAMP1 from...
Hi, what is the value of HSE on nucleo nano board stm32l432kc ?​​https://www.st.com/en/evaluation-tools/nucleo-l432kc.html#overview​Future : 24MHz crystall​But when I initialize default settings in cubemx it sets HSE as 8 MHz.​​Cant find value of HSE...
How to connect to UART via USB on android device? Do I need some driver on android device?​Stm32L432KC nucleo​
Kudos from