STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32h7 vddldo on non bga packages

Hello, I was looking for an stm32h7 part where I could provide voltage to the internal ldo from a vddldo pin to achieve lower power consumption using an external smps. I'm looking at the h743 lineup but cannot find any package with such exposed pin e...

AAnci.1 by Associate II
  • 1535 Views
  • 1 replies
  • 0 kudos

Resolved! I am usinng STM32H7 nucleo board. I want to generate 20KHz pwm wave. How can I control the resolution (that is a value from 0-10000 that corresponds to 0-100%)?

 So I adjusted the ARR and Prescalar values to adjust the pwm frequency(20KHz). Timer Clock is 200MHzI want to change the resolution in the run time with a function. How can I change it?Changing the ARR value will change the resolution?Thanks in adva...

VRapa by Associate II
  • 2409 Views
  • 4 replies
  • 0 kudos

QUADSPI timings to read, write, erase flash IC

Hello,I've a MT25QL128 IC interfaced with STM32F767 controller on QUADSPI. there is external crystal of 8MHz. I want to check timings req for read, write and erase the flash IC, so that I can write some data into flash. I've referred application note...

AShel.1 by Associate III
  • 2338 Views
  • 6 replies
  • 0 kudos

Resolved! Overcoming SPI speed limitation on H743- inspiration needed

I'm setting the SPI input clock for the port I'm using at 50MHz to allow SPI speeds up to 25MHz for use with an SD card under SPI. However, this gives a minimum speed of 50MHz/256 = 195KHz and this is too fast for initialising some SD cards. I need t...

PMath.4 by Senior III
  • 2331 Views
  • 4 replies
  • 0 kudos

Flash Sector Resets After Reading for No Apparent Reason

I am writing an application and bootloader to STM32H7.I append some data to the end of the application. My bootloader needs to be able to read this appended data.When my bootloader first writes the application via (erase->write to memory).When the sy...

AAgar.2 by Associate III
  • 1730 Views
  • 2 replies
  • 0 kudos