2020-01-28 9:48 AM
I am working on an automotive product that will interface with the vehicle's CAN bus network running at 500kbps. My question is, is the STM32F446 capable of reliable communication without a crystal? Or is it absolutely necessary? The last thing I would want is the MCU crashing the vehicle's network.
Currently I have the CAN peripheral clock at 45Mhz, Prescaler = 5, TimeSeg1 = 13, TimeSeg2 = 4.
/***********************************************
 * Baud Rate:               500kbps
 * Clock Speed:             45Mhz
 * Prescalar:               5
 * CAN periph. clock speed: 9Mhz => (45Mhz / 5)
 * Time Quanta (Tq):        18 =>  (13 + 4 + 1)
 * Time Quanta seg 1:       13
 * Time Quanta seg 2:       4
 * Time Quanta sync width:  1
 ***********************************************/
 
/* USER CODE END 0 */
 
CAN_HandleTypeDef hcan1;
 
/* CAN1 init function */
void MX_CAN1_Init(void)
{
 
  hcan1.Instance = CAN1;
  hcan1.Init.Prescaler = 5;
  hcan1.Init.Mode = CAN_MODE_NORMAL;
  hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
  hcan1.Init.TimeSeg1 = CAN_BS1_13TQ;
  hcan1.Init.TimeSeg2 = CAN_BS2_4TQ;
  hcan1.Init.TimeTriggeredMode = DISABLE;
  hcan1.Init.AutoBusOff = DISABLE;
  hcan1.Init.AutoWakeUp = DISABLE;
  hcan1.Init.AutoRetransmission = DISABLE;
  hcan1.Init.ReceiveFifoLocked = DISABLE;
  hcan1.Init.TransmitFifoPriority = DISABLE;
  if (HAL_CAN_Init(&hcan1) != HAL_OK)
  {
    Error_Handler();
  }
}2020-01-28 11:32 AM
Pretty sure you need a crystal to hit +/- tolerance on the bus, check specs for CAN bus