STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_Receive() on STM32F407 is receiving only one byte a time irrespective of amount of data being transmitted on transmitter side.

Hello,Am using STM32F407 (Discovery board). This is connected with a PC which is sending 100 bytes of data and realized that only 1 byte is received and remaining 99 bytes are lost. Below is the code excerpt running on STM32F407      while(1)      { ...

DevBee by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos

I am working on stm32g071. In which i am sending some log message from uart3. But after 8 - 10 hour it stop sending data. What could be the possible issue. Please guide. The sample of my main file is given below....

   /* Initialize all configured peripherals */   MX_GPIO_Init();   MX_SPI1_Init();   MX_USART1_UART_Init();   MX_USART2_UART_Init();   MX_USART3_UART_Init();   /* USER CODE BEGIN 2 */   USART1->CR1 |= USART_CR1_RXNEIE_RXFNEIE; ///USART_CR1_RXNEIE;   ...

Dkuma.13 by Associate II
  • 2029 Views
  • 4 replies
  • 0 kudos

Image overlapping flash banks on STM32H745

Hello,We are using the STM32H745 dual core series, and have an image size that is nearing the single flash banks limit of 1MB. We won't be using the swap bank feature at any point. Will there be issues if the image overlaps the second bank?

TypeKazt by Associate III
  • 1139 Views
  • 2 replies
  • 0 kudos

CAN messages lost in the way

Hello Everybody,I'm building a device who need to transfer a bunch of datas on a CAN bus at 250bauds.When I get the datas from my buffer to create the messages, it seem that some are mission (I'm sniffing the CAN bus with a can-bus shield from seedst...

SSchm.5 by Associate III
  • 2115 Views
  • 3 replies
  • 0 kudos

QSPI - Clock starts before chip select is set

HiI am using the QSPI to interface FPGA.The setup includes STM32F769I-EVAL board wired to MAX10 evaluation board.The QSPI is configured to indirect mode, data phase only. I was able to read data from the FPGA, control clock speed and set number of by...

0693W000001srG4QAI.jpg
Arnon by Associate III
  • 2675 Views
  • 4 replies
  • 0 kudos

stm32f767igt doesn't erase the flash

Hi All.I work with stm32f767igt for using flash.The code below is erasing and writing flash.I succeed writing the flash.​But when i try to delete the flash with HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError) ;andFLASH_Erase_Sector(FLASH_SECTOR_10 ...

0693W000001sH6wQAE.png
Glee.11 by Associate II
  • 6673 Views
  • 17 replies
  • 0 kudos

Resolved! Errors with double as function parameter

If i try to create or run a function that uses a double as parameter it will end up in an UsageFault_Handler infinite loop.Why is this and how can i fix this ?(This prevents me even from using round() from math.h)I use System workbench for STM32on a ...

negatic by Associate
  • 1557 Views
  • 2 replies
  • 1 kudos