User Activity

So I was handed code that breaks when debugging, but to fix the breakage breaks a power control on the board. Rev A only has this problem but Rev A is what I'm stuck with . Nice, right? So I need a way to tell at run time whether the debugger is att...
Is it just me or did everyone else just suffer an unwanted unrequested "update" to their IDE?
An oldie but still needed, CRC in the last word of the FLASH segment. So I'm fine up until I get to the point when I tell TrueStudio my application is other than an .ELF because at Properties / Run/Debug Settings/ Edit / TrueStudio is hobbled by supp...
I'm not sure how many H7xx applications deploy without EEPROMs. Everything I've touched in the last 5 years in the F3xx and H7xx line needed an EEPROM for the usual customer side configuration persistence requirement. My customers prefer to take the...
Does one pulse mode offer the complementary output? My complementary output just sits there. I'm on TIM17 and I'm not sure if being on the 'lite' timer is the problem. I suppose I'll try moving it over to TIM2 and see if the problem persists althou...
Kudos from