STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Code runs fine after `st-flash write`, but not after reset

I'm using the template code for the STM32F7508-DISCO from the STM32CubeF7 repository with the only change being that I add a LED toggle and a busyloop to an infinite loop in `main`. The startup code and everything else is per the template.If I flash ...

GSpre.1 by Associate III
  • 3350 Views
  • 5 replies
  • 0 kudos

Resolved! what is the the hardware fifo size of STM32f103CB and how to know whether the FIFO is empty or full?

HiAs the title mentioned, I can't find relevant information in the datasheet.I get some problem when using UART. I have two chips, the master chip transmits packages to RS485 Bus line, and the slave chip receives it then transmits the respond(UART1),...

Olly Kao by Associate III
  • 3565 Views
  • 3 replies
  • 0 kudos

Resolved! Hi, I am new to STM32. I am trying to get the RTC working on a nucleo F302R8 board. But the seconds are giving weird returns. I am not sure that minutes work properly either.

Here is the RTC initialization code:static void MX_RTC_Init(void){ /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ RTC_TimeTypeDef sTime = {0}; RTC_DateTypeDef sDate = {0}; /* USER CODE BEGIN RTC_Init 1 */ /* USER CODE END RTC_Init 1 ...

GPapo.1 by Associate
  • 2461 Views
  • 3 replies
  • 0 kudos

SPI DMA multimaster setup, buffert size issues

HelloIm working on a multimaster setup, but having alot of problems setting it up.the processor in use is stm32f765zgThis is my pin setup(msp):SPI2_SCK_GPIO_CLK_ENABLE(); SPI2_MISO_GPIO_CLK_ENABLE(); SPI2_MOSI_GPIO_CLK_ENABLE(); SPI2_CS_G...

MBohm by Associate II
  • 2236 Views
  • 4 replies
  • 0 kudos

GPS: STM32L010K4 Hardfault_Handler at STM32L0xx_it.c:0x80006

Dear fellow geek, I am working on a project wich uses the STM32L010K4 microcontroller. We implemented the chip on a PCB and we can write pins high and low and we’re able to use SPI.This project revolves around a GPS application. We’re trying to use t...

0693W000003PMTqQAO.jpg
Rgoss.1 by Associate II
  • 4727 Views
  • 10 replies
  • 0 kudos

OTFDEC in STM32L562QE-DK . Creating a simple project out of https://www.youtube.com/watch?v=MUGte7qx9CU example . Any leads ?!

I am a starter with respect to high end controllers.I am having STM32L562QE-DK. I downloaded the OTFDEC_ExecutingCryptedInstruction project out of STMCube. It works as it is.What I tried ?! :I wrote a small code for subtracting two numbers and had it...

VNara.1 by Associate II
  • 841 Views
  • 0 replies
  • 0 kudos

Resolved! Check watchdog status ?

hi , Actually i am using STM32h750 controller. In this i want to know that ,is watchdog expiry occurred / not while main program is in running. After initializing the IWDG the 26 bit in RCC_RSR register is going to set. So how i know by ...

srikanth by Associate III
  • 4147 Views
  • 4 replies
  • 0 kudos