Hi,I'm trying to get SPI_B on the NUCLEO-H7A3ZI-Q to work with low level drivers. But I have no output:This is my code: LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA); LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB); /* SPI1 /CS */ ...
I'm trying to get a nucleo-H7A4 getting to run my code.Only I got this message now: ------------------------------------------------------------------- STM32CubeProgrammer v2.4.0 -------------------------...
When I start the debug environment in stm32CubeIde. I got the following error message:STMicroelectronics ST-LINK GDB server. Version 5.5.0Copyright (c) 2019, STMicroelectronics. All rights reserved.Starting server with the following options: Pe...
Is there an LL example to enable the backup ram. This doesn't work: // Enable PWR clock LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR); // Enable Backup ram clock LL_APB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_BKPSRAM); LL_APB1_GRP1_Enabl...
I'm making my own low level CAN driver. I have a problem releasing the CANperipheral from sleep mode. So there are more requirements then I found so far. LL_AHB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_CAN1);
LL_AHB3_GRP1_ForceReset(LL_APB1_GRP1_P...
I did check for updates. And I got the latest version.STM32CubeIDEVersion: 1.3.1Build: 6291_20200406_0752 (UTC)OS: Windows 10, v.10.0, x86_64 / win32Java version: 1.8.0_202