STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AD7616 SOFTWARE MODE with STM32H743ZI2

Hello,Good day, I am a intern trying to get the AD7616 to work with STM32h743ZI2. My main objective is to use the AD7616 in software mode and convert the analog inputand read them over SPI. The sequence of steps, I will be following are as follows: -...

dawn98f by Associate
  • 2352 Views
  • 2 replies
  • 0 kudos

standby mode current consuption

hello i am working on (STM32L152RETX) .when my mcu goes on standby mode then the current consumption 8.2 micro amp but as a documents standard i required 5.2 micro amp

Asing.3 by Associate II
  • 852 Views
  • 1 replies
  • 0 kudos

How to Core Reset(M7 => M4 or M4 => M7 Core Reset)

Hi..I am using STM32H745.Can I restart the M4 Core on the STM32H745-M7 core, or vice versa, the M7 Core on the M4 Core?It does not matter whether it is a software method or a H/W method supported by a processor.Please let me know if there is a possib...

Nki h.1 by Associate II
  • 2974 Views
  • 3 replies
  • 0 kudos

How to use the on-board accelerometer for beginners?

Hello ST users,I am a beginner embedded coder (Embedded C coder) and i wanna know how do i use the on-board accelerometer of the stm32f4discovery board. I have learnt SPI and I2C and i guess that works on one of these. Please HelpI would really appre...

AUbar.1 by Associate
  • 1479 Views
  • 1 replies
  • 1 kudos

STM32F205RB FLASH operation effect on global interrupts

Hi,I am using internal flash of STM32F205RB . i need to know when the flash read/write operation is going on how the interrupts(global/timer etc..) will be effected.I have seen the data sheet of STM32F205RB but i didn't find the useful information.I...

SNAGU.1 by Associate
  • 1527 Views
  • 2 replies
  • 0 kudos

Data Logger using STM32L0 and SPI Nor Flash file system

Hi All,I am trying to make data-logger using STM32L0, I application demands to store 2Mb data in .txt and .CSV format for that I am using SPI NOR Flash by Winbond W25Q32JV. I have never used SPI Nor Flash before and new to the file system.Please help...

Vijay1 by Associate II
  • 3286 Views
  • 5 replies
  • 0 kudos

STM32F407VG-DISC1 ERROR while validating NN model on target. LOAD ERROR: STM32 - no connected board(s), invalid firmware or the board should be re-started.

Hi, I am trying to deploy a Keras NN model that fits in the board STM32F407VG-DISC1.The model is created and loaded it into the project according to the latest given documentation and latest version of tools is used.While working with STM32CUBEMX and...

MH M.1 by Associate II
  • 1457 Views
  • 2 replies
  • 0 kudos

Resolved! How to get max ADC sample rate on STM32H745?

I am using an STM32H745 and trying to get the ADC to run at 3.333 MSPS. Currently I am prototyping on a Nucleo-144 development board which has a LQFP144 package MCU on it. While according to the datasheet (page 185), I should be able to run an ADC at...

JBerry by Associate III
  • 5038 Views
  • 2 replies
  • 1 kudos