2020-04-09 6:55 AM
I recently bought a nucleo board for a project im making. I have in the past used 8 bit AVR chips but I want to step up to STM32. My project is some switches, leds, a DAC and an ADC. One thing that is common to all these elements is a serial data out. The way I would usually do this is to use a number (let's say 8 bit) to hold a 'walking bit' to count through each bit in a byte, on each count ANDs with the data (also 8 bit) and the output is then sent to the output pin. I am used to programming in C in AVR GCC so I would write something like this -
for(i=0;i<8;i++){ // loop 8 times
COUNT <<= 1; // left shift walking bit
if (COUNT & DATA) { // compare data and walking bit
PORTA |= 1<<0; //set output if data is high
} else {
PPORTA &= ~(1<<0); // clear output if data is low
}
}How do I achieve the same thing with my nucleo? I am most used to using bare C, but I don't know how to code this for STM. I am happy to use CMSIS or HAL, whatever is closest to what I know already.
any help much appreciated
2020-04-09 8:18 AM
Enable the GPIOA clock, configure the GPIO pin as a Push-Pull Output
for(i=0;i<8;i++){ // loop 8 times
COUNT <<= 1; // left shift walking bit
if (COUNT & DATA) { // compare data and walking bit
GPIOA->ODR |= 1<<0; //set output if data is high (PA0=1)
} else {
GPIOA->ODR &= ~(1<<0); // clear output if data is low
}
}
More efficient would be to use the Set/Reset register
for(i=0;i<8;i++){ // loop 8 times
COUNT <<= 1; // left shift walking bit
if (COUNT & DATA) { // compare data and walking bit
GPIOA->BSRR = 1<<0; //set output if data is high (PA0=1)
} else {
GPIOA->BSRR = 1<<(0 + 16); // clear output if data is low (PA0=0)
}
}
2020-04-09 8:48 AM
thanks! that looks a lot closer to what I know already than I expected.
when you use BSRR for the output, you're not using HAL, does that mean you're using CMSIS? I'm trying to understand the difference between HAL, CMSIS etc.