STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HI, i am doing project on fan controller , i need to measure power factor between my voltage waveform and current waveform which is generated on my CRO. i need to write code to display the powerfactor value. should i use input capture method .

or else do i need to set two GPIO pins as EXTI with rising edge interrupt.i am already generating two waveforms with some dealy . But should i use Input capture method to capture the values at rising edge at each pulse and need to count the number o...

Lchal.1 by Associate III
  • 849 Views
  • 0 replies
  • 0 kudos

STM32F746 Discovery QSPI Memory mapped mode issue

Hello, I want to use external QSPI flash memory micron n25q128 in Memory mapped mode  STM32F746 Discovery. I used below code to make external flash in memory mapped mode but I can see incorrect data at external flash. I am not sure whats wrong in m...

Byte loss in DMA based SPI slave implementation

We are using STM32L475RE as SPI slave and TI based DSP as master. We are operating the SPI at 1Mhz clock frequency.We are seeing intermittent data loss in the transmission when data size is high. We observed that the HAL_SPI_TransmitReceive_DMA call ...

gota by Associate II
  • 842 Views
  • 0 replies
  • 0 kudos

CAN doesn't works (STM32F767ZI)

Hi everyone,I use STM32F767ZI nucleo board and i'd like to use CAN to send data.To begin ijust want to see the data frame sent on Can_Tx on my oscilloscope.For this i just connect the Can_rx to the Can_tx of my nucleo board on PD0 and PD1 to see what...

0693W000003Bp10QAC.jpg
Uvess.1 by Associate II
  • 4865 Views
  • 11 replies
  • 0 kudos

using the TIMER2 ETR input in reset mode for stm32F446RE

Hi everybody,i would like to use the STM32F446 Timer2 with one external input to reset the counter (avlue to 0), then having an input capture to read the timer value between two consecutives reset thru ETR input. Input capture settings is not a probl...

papageno by Associate III
  • 3142 Views
  • 5 replies
  • 0 kudos

I cant write to the FLASH OPTION register

Hi allI need to write an external programmer for STM32G030J6.I've written the SWD protocol, and I'm able to program all FLASH (if no protection applied).the issue is: I can’t write to the FLASH OPTION: (changing protection level from 1 to 0) I can’t ...

YWhit by Associate III
  • 1349 Views
  • 2 replies
  • 1 kudos

Resolved! Wake up STM32G030K6T from stop mode using wake up pin

I could wake up the controller from stand-by mode but I realized I needed to use stop mode. What needs to happen for the controller to wake up from stop mode when using a wake up pin? Do you have some code examples preferably using the HAL functions?

varo1111 by Associate II
  • 1886 Views
  • 2 replies
  • 0 kudos

Support for Unicleo-GUI-STM32MCU

Dear TeamGone through the user manual,refer the below linkhttps://www.st.com/content/ccc/resource/technical/document/user_manual/group0/b9/d0/7c/c5/a8/55/4c/bc/DM00337036/files/DM00337036.pdf/jcr:content/translations/en.DM00337036.pdfAlso find the b...

SS_135 by Associate II
  • 1161 Views
  • 1 replies
  • 0 kudos