STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

smartcard application transform stmf4 series to stmf7 series

Hi, I have an application on STM32F4 MCU which is based on Smartcard T =1 protocol according to ISO 7816. The app works very well. Then I choose other STM32F7 board to test this application, i faced with problems, i can read ATR from SmartCard but i ...

0693W000003QdKEQA0.png
D.eknc by Associate
  • 721 Views
  • 0 replies
  • 0 kudos

Is the STM32F103xG CAN bus suitable for Unpowered Node use?

Some sources state that some CAN transceivers disable the entire bus if their node is powered-down (due to low-impedance while unpowered).Some manufacturers (e.g. Texas Instruments, Microchip) explicitly state in some datasheets that their transceive...

RJone.1 by Associate
  • 620 Views
  • 0 replies
  • 0 kudos

Resolved! UART Transmission error (to computer using FTDI board )

I'm trying to UART Transmission to computer using FTDI board with below [Environmets.]But it have a [problems] like below..Please, let me know the reasons and solutions..:sad_but_relieved_face: [Environments​]MCU : STM32L432 Nucleo-32 boardFTDI Board...

JShim.1 by Associate
  • 3645 Views
  • 2 replies
  • 1 kudos

Resolved! stm32 USART2 issue

Hi , My USART1 works fine when i send a character and i recieve a character in comport , but i need to also configure USART2 ,i have configured the apb1 register and also apb2enr for the GPIOA clock enable ,i know for the fact that the clock on apb1 ...

Oahme.1 by Associate III
  • 1925 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F407 DMA and ADC bare metal

HiI am trying to get my ADC measurements of the interal chip temperature and data transfer to a global variable via DMA working properly. The ADC1 is triggered every second via timer 4. Configuration is stream0, channel channel 0. I do get several er...

AAnth.1 by Senior
  • 4553 Views
  • 5 replies
  • 0 kudos

Resolved! I cant access ADC values from DMA buffer into any other variable in while loop. DMA buffer have values in it but not going into other variable. Can anyone tell me where im wrong????

/* USER CODE BEGIN Header *//** ****************************************************************************** * @file      : main.c * @brief     : Main program body ****************************************************************************** * @at...

0693W000003QWqIQAW.png