STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I am using NUCLEO-64 STM32F401 and I have attached a serial EEPROM to I2C3. I am using the LL library calls to try to write to the EEPROM but I cant get the slave address to appear on the I2C bus. I do see the start pulse on the scope. Code below.

The code below gets stuck at --- while (!txBytes) txBytes=LL_I2C_IsActiveFlag_ADDR(I2C3);and the ADDR bit never gets read as set?==========================================void I2C_Write(uint8_t dataCount, uint8_t data){ uint8_t I2CAddrWrite = 0xa0;...

DCull.1 by Associate
  • 862 Views
  • 0 replies
  • 0 kudos

Program gets stuck in for loop after interrupt runs

This has me scratching my head - my program runs fine UNLESS the interrupt occurs, after which it gets stuck in a for loop near the start of the program. I can't see any way these two things are connected with each other - there dont share variables....

deep_rune by Associate III
  • 1655 Views
  • 5 replies
  • 0 kudos

SPI communication between f030R8 (slave) and ESP32 (master)

HelloI am trying to setup SPI communication between an ESP32 as Master (programmed with arduino ide) and an f030R8 programmed with the Cube IDE. The stm is reading analog values from its adc pin in the main loop and should transmit them to the master...

Cmuel.1 by Associate
  • 2912 Views
  • 0 replies
  • 0 kudos

STM32F427 is sometimes running slow after boot

I have an issue with STM32F427 where after doing reset for MCU in some cases the MCU is running at about half the speed after reset. All peripheral clock seem to be running at normal speed, but the MCU is just running at half the speed. All register ...

Resolved! Starting a Timer via a GPIO Pin at a changing edge and return the value into the DMA via another GPIO and changing edge

Hey,I'm using a Nucleo-F446RE and the STM32 Cube IDE.I want to start the Timer3 with a changing Edge at a GPIO Pin. Then the Timer should count till another GPIO has a changing Edge aswell. Now the timer should be disabled and the counter should be s...

MHerz.1 by Associate II
  • 4247 Views
  • 5 replies
  • 0 kudos

How to trace the data in SWV using STM32F303RE Nucleo board?

Actually, I could able to debug the STM32F303RE Nucleo board and could see the value of the variables by keeping the breakpoint while debugging.Instead of keeping the breakpoint, I want to trace the value of the variable using SWV and also I want to ...

PDeva.1 by Associate
  • 1629 Views
  • 1 replies
  • 1 kudos

STM32H745 - SPI doesn't transmit any data. - SOLVED

SOLVED - look at edit below!I am trying to implement SPI on nucleoH745ZI-Q without HAL or any kind of driver, I wrote my own registers pointers and functions like digitalWrite, pinMode or printf. I set up RCC, GPIO and SPI registers (all set, checked...

0690X00000BvSgSQAV.jpg 0690X00000BvTBpQAN.jpg