Associate III
May 10, 2020 8:15 PM UTC
Question
STM32 F4 Timer Input capture
- 2 replies
- 875 views
Dear community,
I am trying to use a timer to see if there is no activity on a data line. However, it works not as expected.
As you can see in the picture, the timer (yellow) gets interrupts when the signal line (pink) is changing. But no interrupt, when there is no change. I want the opposite.
See my configuration below.
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_IC_InitTypeDef sConfigIC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 2;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 500;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_IC_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_FALLING;
sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
sConfigIC.ICFilter = 0;
if (HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
HAL_TIM_IC_Start_IT(&htim2, TIM_CHANNEL_1);
/* USER CODE END TIM2_Init 2 */
}void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Instance == TIM2) {
__HAL_TIM_SetCounter(&htim2, 0); //reset counter after input capture interrupt occurs
}
}void TIM2_IRQHandler(void)
{
/* USER CODE BEGIN TIM2_IRQn 0 */
HAL_GPIO_TogglePin(DSP_RST_GPIO_Port, DSP_RST_Pin);
//HAL_GPIO_WritePin(DSP_RST_GPIO_Port, DSP_RST_Pin, GPIO_PIN_SET);
/* USER CODE END TIM2_IRQn 0 */
HAL_TIM_IRQHandler(&htim2);
/* USER CODE BEGIN TIM2_IRQn 1 */
/* USER CODE END TIM2_IRQn 1 */
}