STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745 - SPI doesn't transmit any data. - SOLVED

SOLVED - look at edit below!I am trying to implement SPI on nucleoH745ZI-Q without HAL or any kind of driver, I wrote my own registers pointers and functions like digitalWrite, pinMode or printf. I set up RCC, GPIO and SPI registers (all set, checked...

0690X00000BvSgSQAV.jpg 0690X00000BvTBpQAN.jpg

Resolved! DMIE typo (should be DMEIE)

In RM0430 Rev 8, 9.3.19 DMA "Error management":an interrupt is generated if the corresponding interrupt enable bit (TEIE, FEIE, DMIE) in the DMA_SxCR or DMA_SxFCR register is set.It should say "DMEIE", not "DMIE"

Miles1 by Associate III
  • 1184 Views
  • 1 replies
  • 0 kudos

Cannot copy bin data to Nucleo-F072RB.

Hi We have bought a Nucleo-F072RB board and tried to set up it following STSW-STUSB001 user manual.Currently my process is till "Drag and drop of the configuration file (NUCLEO_F072RB_STUSB_NVM_config_1.6.bin) to STM32 Nucleo drive".Situation is as ...

KHiga.1 by Associate
  • 1048 Views
  • 1 replies
  • 0 kudos

How to perform CQ overload test using l6360.

Hi,I am using STM32f423RH and l6360.how to perform CQ overload test..?I am able to read and write the registers of l6360.As per my understanding from the data sheet, CQ overload will happen when the CQ line reaches the cutoff (programmed cutoff) then...

SNAGU.1 by Associate
  • 747 Views
  • 0 replies
  • 1 kudos

STM32F746NG DISCO DMA Quad-SPI flash memory example.

I believe the QSPI Flash memory is in the memory mapped mode on the DISCO board. I programmed a 2KB bin file into the flash memory using the ST Link utility. I want to read this to internal ram. I set this project up with CubeMX. Can I change the fla...

Resolved! CAN setup on STM32F303

I've been working with CAN on the STM32F1 for some time , but I'm having a terrible time trying to get it to work on the F303. I'm hoping someone can tell me what I'm doing wrong. Thanks very much for looking at it.void can_gpio_config(void) { GP...

Resolved! Why voltage drops while using GPIO as a timer input

Greetings.I've entirely stuck with this problem.MCU: STM32F407VGT6Realization: custom PCB and F4 Discovery board.Problem: Microcontroller can't gather information from encoders.Description:   There are three motors with built-in encoders that I want ...

PWM Timer generation not working with low duty cycle

At low duty cycle (like below 5%), the timer pwm stops periodically (see the attached picture). The higher the duty cycle, the smaller the stop period. Does anyone know why this happens?For context, I am using the STM32F072 Discovery board. I use Cub...

0693W000003RBXMQA4.jpg
vtran1 by Associate II
  • 2920 Views
  • 5 replies
  • 0 kudos