STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What's the best way to do bit-banging with timers and DMA?

Hello,I want to implement VGA signal generation on my STM32L432KC board. For start, getting the vertical sync and horizontal sync timings right would be great. I found a nice website with hsync, vsync and pixel timings and I thought that using resolu...

PPles.1 by Associate
  • 3289 Views
  • 4 replies
  • 0 kudos

Problem with external GPIO interrupts on STM32G030K8.

Configuration Info:MCU : STM32G030K8STM HAL Dirve Version : 01.03.00.00 PA4 (GPIO_PIN_4) - Configured to generate interrupt upon detecting a falling edge. PB5 (GPIO_PIN_5) - Configured to generate interrupt upon detecting a falling edge and rising ed...

Tkamaal by Associate II
  • 2610 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F030R8T6 ADC Calibration Error

i am using Nucleo-F030R8 board. I want to get adc calibration factor.By writing #define VREFINT_CAL (*((uint16_t *) 0x1FFFF7BA))i got VREFINT_CAL = 1521 which is actually factory stored value, that good no problem.but when i try to calibrate it by...

sanju by Senior
  • 1467 Views
  • 6 replies
  • 0 kudos

Resolved! How to change Synchronous Pre-Divider

I am using an F4 discovery board and trying to using the included 8MHz HSE crystal to drive the RTC. I am using CubeMX to configure everything and I have configured the RTC to generate the calibration 1Hz signal that I am watching on a scope. Initial...

JScri.1 by Associate
  • 3704 Views
  • 2 replies
  • 1 kudos