cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to flash STM32 Nucleo board then power it with a battery and use it in an application without connecting it to PC?

LMoha.1
Associate II

Is it possible to flash STM32 Nucleo board then power it with a battery and use it in an application without connecting it to PC?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

Sure. The board doesn't care what is powering it. Probably needs to be connected to a PC to flash it.

If you feel a post has answered your question, please click "Accept as Solution".

Yes but i flashed a small program of blinking the green led of the Nucleo via ST link Utility! but nothing happened ! i can't see the led blinking, however i can see blinking with debug mode (via STM32CubeIDE) !

TDK
Super User

How exactly are you powering the board? There are guidelines in the user manual for valid power configurations. The ST-Link chip could be holding the other one in reset if not done correctly.

If you feel a post has answered your question, please click "Accept as Solution".