STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I am completely new to STM32 MCU programming. I am trying to make a simple variable frequency complementary square wave generator with my STM32F103C8T6 blue pill to drive an inductive load. I'd like to use a potentiometer to vary the frequency.

Frequency range I'm looking for is from 60 kHz to 200 Khz. Here's the code I generated with Cube IDE. It initializes the GPIOs, ADC, and PWMs but I don't know how to integrate a potentiometer in this code and be able to vary the frequency of the comp...

SGulc.1 by Associate
  • 1315 Views
  • 1 replies
  • 0 kudos

TTCAN in STM32F767

Hello I have read on the reference manual that the CAN controller can be set to work as TTCAN by setting the TTCM bit. But comparing with the STM32H7 it seems that only the latter family has the TTCAN functionality.Someone has experience with that ?R...

DVicc.1 by Associate II
  • 1196 Views
  • 1 replies
  • 0 kudos

STM32F7 RTC Accuracy/Calibration Methods?

Hello Everyone, I am using the STM32F777 and utilizing its RTC and external 32.768 crystal(LSE).Currently I am having a drift of 79s in 76 hours. it is a little bit less than a second per hour. It is not that bad but I would like to have a better res...

Mauricio by Associate II
  • 1408 Views
  • 1 replies
  • 0 kudos

Unstable Current Consumption in Low Power Mode

Greetings From Turkey, We have a hardware using stm32l471. We wake up at certain times and send data to the server. Then we go back to sleep mode.Here is the our callback to switch to low power consumption mode.void low_power_callback (int time) { s...

VÜnal.1 by Associate II
  • 1700 Views
  • 2 replies
  • 0 kudos

Resolved! Preserve a section of FLASH memory during programming

Following in the directions of this post, I am able to reserve and write to (and read back) from a section of FLASH dedicated to calibration data. However, when I reprogram the device, the IDE wipes the whole memory clean before programming and we lo...

JMill.1 by Associate III
  • 4945 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO-H743ZI2 ADC Polling gives wrong result.

Hello,I am trying to read single ADC channel using NUCLEO-H743ZI2 board but the result is wrong. I have created a very simple project using CubeMX. Kept the default Clock setting. Enabled ADC3 CH0 (PC3_C Pint) in single ended mode polling. Enabled UA...

ABane.1 by Associate III
  • 3241 Views
  • 7 replies
  • 0 kudos

Resolved! STM32H750 ignores pull-up resistor when EXTI is selected

On F1xx and F4xx platforms, I have been using the GPIO pull-up resistors for the connections to OC hall sensors used in BLDC motors. There has never been a problem. With STM32H750, I can see that the PUPDR register has the right values for the pull...

olavi by Associate III
  • 2724 Views
  • 7 replies
  • 0 kudos