cancel
Showing results for 
Search instead for 
Did you mean: 

F730 flash PSIZE vs. Supply voltage

RMcCa
Senior II

I am a bit confused by the language in the F7 reference manual, section 3.3.5 (RM0431) that describes the flash program/erase parallelism. Does the power supply limit the maximum value of the parallelism or does it limit one to a particular size?

The caption for table 6 is "Table 6 provides the correct PSIZE​ values". Should it say "correct maximum PSIZE values"?

I am asking because i have been writing bytes to the flash with Vcc=3.3V and PSIZE = 0 and its been working fine for a while​, but i wonder if that's only luck and i should switch to 32bit writes. Speed is not an issue in this case.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
RMcCa
Senior II

I know this is minor, but i also found a few copy & paste errors in stm32f7xx_hal_flash.c when i was looking for the answer. The @note in the comments is incorrect for FLASH_Program_Word​, Halfword & Byte.

View solution in original post

17 REPLIES 17
Uwe Bonnes
Chief

"correct maximum PSIZE values" is the right thing

Uwe,

Can you please quote a source for this?

@Imen DAHMEN​ ,

Can this please be clarified, across all STM32 RMs?

Jan

Imen.D
ST Employee

@RMcCa​ , It's ok for your use case. I confirm, it is the max PSIZE vs Voltage.

I will raise this internally to update all STM32 RMs.

Edit: We suggest to change “Parallelism size�? to “max parallelism size�?.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
RMcCa
Senior II

Thank you, good to know my code wasn't working by accident.​

RMcCa
Senior II

I know this is minor, but i also found a few copy & paste errors in stm32f7xx_hal_flash.c when i was looking for the answer. The @note in the comments is incorrect for FLASH_Program_Word​, Halfword & Byte.

The datasheet STM32F730x8 page 127, table Table 53. Flash memory programming (continued) seems quite clear to me.

Interesting. There is an additional mistake then. The datasheet list 3V max for 32bit programming while the RM says 3.3V.

Yes, the max value for 32-bit program operation seem wrong

Thanks, Imen.

Jan

@Imen DAHMEN​