STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use Oversampling with H753 ADC..

I've been trying to get Oversampling working using polling for ADC completion, but I'm not seeing the expected results. I found one example for x4 oversampling, but in reality that doesn't seem to actually be doing anything. I am trying to use 32 f...

BBick.1 by Associate II
  • 1545 Views
  • 2 replies
  • 0 kudos

微型太阳能逆�?�器

微型太阳能逆�?�器有评估�?�?微型太阳能逆�?�器控制软件是�?��??供给用户?或者有开�?�“微型太阳能逆�?�器�?的朋�?�和我�?�系?我的邮箱:

SQian.1 by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos

Need help setting up DMA on STM32F1 & F4

Hi, I am trying to set up an input capture with DMA on a F1 and a F4 chip. The documentation is confusing, and most tutorials don't work for my specific scenario. For a start, when setting up DMA using cubeMX, I can't configure source, destination an...

Ubus99 by Associate III
  • 3052 Views
  • 6 replies
  • 0 kudos

Changing GPIO pin from PWM to Digital Output at run time

Hello, in STM32F10x, I need to use Stop mode. However, before going to stop mode, I need to stop PWM channels and leave them high (in output). How can I stop change some pins (A0 and A6) from timer PWM mode to normal output mode? I tried this method ...

GunkutA by Senior
  • 3637 Views
  • 5 replies
  • 0 kudos

Keeping Signed and Unsigned Variables or Values

I wonder about the keeping signed and unsigned values in proccessor.For example I have this define#define MY_NUMBER 8How to decide MCU number of "8" signed or "unsigned" value.How to convert binary number to keeping. For example I am doing static ana...

DCtech by Associate II
  • 1262 Views
  • 1 replies
  • 0 kudos

Resolved! How much flash the BSP_QSPI_Erase_Block() erases ?

I am using STM32F769I-DISO board with an MX25L51245G QSPI chipAs I understand it, I must erase before writing. So if I have 100 bytes of date on the QSPIand I want to change byte number 51 in my 100 byte data I should first eras this location.Howev...

ICohe.1 by Associate III
  • 2730 Views
  • 3 replies
  • 0 kudos

Peripheral to peripheral DMA.

Hi all,I'm triybg to send data to a TFT from an external flash memory.I read than it is possible to comunicate 2 SPI peripherals trough DMA.I dont understand all the thing yet. Please can someone answer this:Lets say Flash is in SPI1 and TFT in SPI21...

JAlca by Senior
  • 1575 Views
  • 3 replies
  • 0 kudos

Resolved! PSoc as I2C Master and ST as I2C Slave

Hi,I want to implement I2C communication between PSOC and ST.I've configured PSoc as I2C Master and ST as I2C Slave. I've succesfully transferred data from PSoc to ST but I'couldn't read data from ST.Here's the details about my implemention.When I us...

0693W000004JKqHQAW.png 0693W000004JKrEQAW.png 0693W000004JKrJQAW.png 0693W000004JKrOQAW.png
HHOKE.1 by Associate
  • 2177 Views
  • 1 replies
  • 0 kudos