STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103C8 Firmware Update over BLE

Hello everyone,We are using the STM32F103C8 connected with the Microchip RN4871 BLE module over UART1. We would like to update the firmware of the STM32 CPU over BLE but we are encountering a few issues. Our BLE module, although it works great for ou...

ZPapa.1 by Associate II
  • 925 Views
  • 0 replies
  • 0 kudos

I have a problem with configuration the TIM1-ETR in stm32f1

I want to use the external clock mode 2 but it dose not work ,configure the PA12 that connect to TIM1-ETR AND make push button pull down to send pulses to that pin(PA12) to detect high edge and make up count to the variable "upCount" in the code ,i t...

HSale.1 by Associate
  • 1346 Views
  • 0 replies
  • 0 kudos

STM32H7 - Handling with 2 MPUs

Hello, the STM32H7 (dual core) has two dedicated memory protection units. If I configure one MPU to make a memory region only accessable as readonly, does the memory protection unit from the other core inherit those configuration or is it bypassing ...

PButc.1 by Associate II
  • 3509 Views
  • 6 replies
  • 0 kudos