STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cable length limitation for SPI run at 40MHz ???

I had trouble to activate SPI communication with SPI in 40MHz frequency in 55cm long cable , even I modified output speed to "Very high speed" . Is any other register that I need to set to support high speed clock in long length cable ? 55cm long cab...

AShiu.1 by Associate
  • 1445 Views
  • 1 replies
  • 0 kudos

Several question regarding STM32Fx (TIMx,DMA,ADC)

Hello,I have few questions regarding the TIMER capabilities confgured as input capture. According to the reference manual, the direct input capture of TIMxCH1 in conjunction with a TMxCH2 which is configured as "indirect input capture mode" along ...

PButc.1 by Associate II
  • 2307 Views
  • 3 replies
  • 0 kudos

Use STM32H743II with an external ldo for vcore @ 400MHz

We would use a STM32H743II with an external ldo for vcore. In the datasheet are tables (page 114, table 31) with regulator on but no tables with regulator off.In the datasheet at page 114 is a table (table 31) for maximum current vs. junction tempera...

Resolved! Using an ADC how can I make the value of Vref- depend on the value of another input on a STM32H742 chip?

I need to implement an ADC to measure phase voltages, so I want to set the N phase as Vref- and get the values of other 3 phases (comparing with N phase) on the output of the ADC. I am using single-ended mode.Is it possible to do this? How can I do i...

EEtxe.1 by Associate II
  • 1886 Views
  • 4 replies
  • 0 kudos

We are trying to get UART-receiver to work in interrupt mode.

Here is the code that doesn't work. Any suggestions?UART_HandleTypeDef UartHandle;uint8_t MyRxBuf[ 10 ], MyTxBuf[3];int main( void ) {  uint32_t t_print;  int16_t i;  HAL_Init();  SystemClock_Config();   /* Put the USART peripheral in the Asynchronou...

RLind.2 by Associate II
  • 1768 Views
  • 3 replies
  • 0 kudos