cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 F446ZE - Board MB1162B-02

HKuma.1
Associate II

I 'm using this board for CAN communication with CAN1. I notice in User manual UM1871 Figure 14. MCU 1 CAN1_TX is connected via SB18 and it is open. For CAN1_RX it is mentioned in user manual that I have to close for Rx to work and not mentioned about Tx pin. Do I need to close SB18 for CAN TX to work and it is missed listed in user manual. Please respond.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
YS.K
Associate III

https://www.st.com/en/evaluation-tools/nucleo-f446re.html

[Tab] Resource -> Schematics

https://www.st.com/resource/en/schematic_pack/nucleo_64pins_sch.zip

STM32 Nucleo (64 pins) schematics

You can check the pin connection in the development board circuit diagram.

HKuma.1
Associate II

Thank you for your response. I'm using STM32F446E board and not STM32 Nucleo