STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Develop digital power with STM32G4 ,using a voltage control and a current loop.How could one FMAC realise two contorl loop?

In STM32CubeG4 Firmware Package, the G474 digiatal power demo use a FMAC to contol a buck or boost toplogy with one voltage control loop.So if I want to use two loops,one for voltage and other for current loop, could the FMAC(in my opinion,that is j...

ZYu.1 by Associate III
  • 951 Views
  • 0 replies
  • 0 kudos

Resolved! Distinguish GPIO port from external interrupt

Hello,I'm some confused how external interrupt is working with GPIO. If PA3 and PB3 are both configured as external interrupt, and assume the two interrupts are not coming simultaneously, how to determine which PIN generates the interrupt when EXTI3 ...

XLei.1 by Associate II
  • 2359 Views
  • 2 replies
  • 0 kudos

CAN bit timing options?

I've been using the following two bit timings for a CAN bus speed of 500K on the STM32F103. I was just wondering which is better? Does it make any difference? Is there another preferred option? Thanks a lot for any insight. //(1+9+8)*4 = 72 //1+9+...

stm32 spi half-duplex transmit into receive mode

the target type is stm32f072, firstly the master transmit data success, slave receive data ok; should i need to disable spi ,enable BIDIOE in slave. but the slave can't transmit data, how to solve it?

Staly.1 by Associate III
  • 3876 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H743ZI SPI Fault/Freeze when reset

Hello Everybody,I am using the STM32H743ZI chip with STM32CubeIde. I have been having success with my code running in debug mode with the debugger attached. however when I power off the board and start it up there is a problem when the program start ...

TCash.1 by Associate III
  • 1344 Views
  • 1 replies
  • 0 kudos

Resolved! Maximun speed of interruptions on STM32F429

Dear all,I need geneate an interruption about 5Mhz to access to an external device using FMC. I am trying to use a Timer to generate that interrupt but I do not get the results I expect. On STM32F429 and STM32CubeIDE, I config timer 10 with the foll...

Resolved! How to send ADC value to serial port via UART.

I'm getting value from LM35 sensor and i am converting it to celcius. Then I am trying to send it to serial port via UART but i couldn't do it. What codes should i use to convert data to bits. Thanks.

sangarius by Associate II
  • 2460 Views
  • 3 replies
  • 0 kudos

Resolved! Diode D20 purpose?

D20 separates Field GND from PGND. Why?Is it recommended for the CLT-01 or the VNI8200XP or both?What is the probable drawback of connecting the 2 nets without this diode protection? 

0693W000003RtbrQAC.png