STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to Receive uint8_t hex via USART?

I tried to receive hex data from my pc terminal to my stm32 but it was not receiving it properly Kindly help me how to Receive the hex value from the PC terminal.

Sprak.11 by Associate II
  • 1894 Views
  • 2 replies
  • 0 kudos

Resolved! Troubles changing boot1 address in Flash Option Bytes

Hello,I am having troubles changing boot1 address in Option Byte in FlashI want to change boot1 address, allowing me to launch either in bootloader mode (system memory) or usercode mode(flash) without using a jump.I am currently testing on the STM32H...

BNord.1 by Associate III
  • 1098 Views
  • 1 replies
  • 0 kudos

Resolved! How to run code from RAM in stm32h7b3i using CubeIDE.

HiBy changing linker script file of GPIO_Toggle code such that it points to RAM . And loaded the .hex and .bin ( specifying start program address as 0x20000000 ). The code looks like get stuck and never toggles LED. But when run in debug mode through...

Skuma.6 by Associate II
  • 1849 Views
  • 2 replies
  • 0 kudos

Matlab Digital filter not working, how come?

Before reading any further, to give you on some insight on the output level of the oscilloscope picture'sthe ~340mV green signal is normal. If you know me I posted a question as to why its 340mV but for sake of simplicity 340mV is normal in this case...

0693W000004KTAzQAO.jpg 0693W000004KTAfQAO.png 0693W000004KTAkQAO.png 0693W000004KTApQAO.png
CLeo.1 by Senior II
  • 1321 Views
  • 1 replies
  • 0 kudos

HAL_UART_Transmit_IT only send first letter

I am very new to use hal_usartTransmit_it because I use only usart_transmit() , which is the blocking mode.I changed all of my transmit() code to transmit_it() for better performance, but after that my ble send message only shows buffer's first lette...

DU2 by Associate II
  • 2540 Views
  • 1 replies
  • 0 kudos