STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_Receive_DMA has an unfindable hickup.

Hello,I'm working with UART Communication between a RPi and an STMG070RB. For the UART communication I'm using the library function HAL_UART_Receive_DMA.I have an initialize in which the Receive function waits for 3 bytes to be received (My messagehe...

JNieu.1 by Associate II
  • 8313 Views
  • 4 replies
  • 0 kudos

Resolved! style RM0316

RM0316The reserved space is clearly indicated at the top, and the style changes abruptly on the next page, and the reserve is no longer specified. what is the result of missing addresses ? why can't a single style be maintained ? for clarity.

Add CubeMX support for dual buffer DMA in ADC modes.

This is a suggestion, not a question...There's no support for dual buffer DMA mode in the ADC HAL, and it would be very easily added.Already did my own copying the existing function for the multimodeDMA.The problem is that CubeMX will wipe the code a...

Is there any required external circuitry for the ADC?

I am using a current sense amplifier (INA190) to measure current. The output of the current sense amplifier will go to the input of the ADC on the STM32. The output range will (ideally) be between (0-VREF). From working with an external 16 bit ADC, I...

JAlle.2 by Associate II
  • 1647 Views
  • 1 replies
  • 0 kudos

STM32F746G-DISCO SDRAM trouble

Hello everyone, I've an STM32F7 Discovery Board. I've been playing with all of the peripherals such a USART, I2C, GPIO, LTDC and SDRAM. And, I've been problems with this last one. I want to do enphasis in that I use to program the device with Atollic...

Jde C.1 by Associate II
  • 2713 Views
  • 6 replies
  • 0 kudos

Calculate number of RTC ticks MCU spends in STOP2 mode

I want to calculate the actual time the CPU spends in STOP2 mode.I wake up the MCU either by RTC Alert or LPUART.The issue is more relevant to LPUART wake use case, because it could happen before the RTC alert expires.I'm using RTC with LSI which con...

deckhard by Associate III
  • 4455 Views
  • 13 replies
  • 0 kudos

Which is the flash configuration of STM32 H7 42 xG ?

Data sheet says: (ch 3.3.1 on page 26)• A user Flash memory block of 512 Kbytes (STM32H7xxxG) or 1-Mbyte (STM32H7xxxI) containing eight user sectors of 128 Kbytes (4 K Flash memory words)which is missing a clear statement for the xxxG variant.Is it f...