Resolved! How to sense JTAG/SWD connected?
How could I in code sense that something is connected to the JTAG/SWD connector?
Ask questions, find answers, and share insights on STM32 products and their technical features.
How could I in code sense that something is connected to the JTAG/SWD connector?
Hello,The HAL_RCC_OscConfig does not return HAL_OK after initializing LSE. I tried removing the LSE from Oscillatortype and worked just fine. Also have USART output and clearly it gets stuck at at OSC initialozation.Here is the USART output:[2020-11-...
I use a CAN BUS gyroscope in my project, I connect it via tja1050 with my MCU(stm32 f103RCT6).I believe that the hardware connection has nothing wrong, and I can see the signals on the BUS using oscilloscope . However, I can't go into the CAN BUS rec...
I'm in a fair ways over my head here. I figured out how to build a STM32F413 program that interfaces with a uBlox GPS receiver over a UART serial port. Now I'm trying to build that code into a C++ class that gets instantiated in my main application. ...
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_7); //PA7 is no longer GPIO interrupt sourceHere is my code to go into timer mode:/*ReConfigure GPIO pin : PtPin */ GPIO_InitStruct.Pin = Vib_In_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull ...
Here is the code of what i am doing, certainly I am still confused where do I have to change the register. #include "main.h" /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; DMA_HandleTypeD...
I'm trying to configure Bank 1 of the FMC in Mode 1 (SRAM). I'm nearly there but ran into a frustrating problem, where it insisted on writing 64 bytes despite me setting the FMC's MWID register to 01 (16 bits) and using a uint16_t* in C to perform th...
The STM32469I-EVAL has 128Mbits NOR FLASH (PN: S29GL128S90FHI0) and 128 Mbits SDRAM (PN : IS42S32800G-6BLI).There is 512Mbits FLASH version of the S29GL family but the access time is higher. Is it an issue for the STM32F469 ?Which requirements have I...
Hello STM Community!First of all, I would like to thank you to read my topic and enter in this discussion.I'm new with STM32, and it's the first project of mine that I really need to worry about energy comsuption.In my project I have sensor that I...
Hello,I am looking into the ROM tables on STM32F439ZI. TPIU (0xE0040000) class type is 0x9, in its romtable, there are two entries:0xb, which is strange because it is marked as present (0b11) but offset is zero which is prohibited.0x1, which means pr...