STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB C Power Role swap by STUSB1600

Hi ,We are making one android accessory which required to pass through power support from accessory to android smartphone.Now we also want to communicate with smartphone by keeping our accessory in device mode.So by using STUSB1600 , Can I do data / ...

PVala.1 by Associate II
  • 2203 Views
  • 3 replies
  • 0 kudos

Generate velocity curve

Hi, I am a NUCLEO STM32H743ZI2 and I am trying generate one velocity curve with the register ARR. I'm using 3 stepper motors and firstly I tested the code with constant velocity but when I increment the velocity from 0 rpm to 2 rpm by 0.001 and the s...

SRivi.1 by Associate II
  • 1057 Views
  • 1 replies
  • 0 kudos

What Nucleo L476rg GPIO output mode should be used, to appropriately drive the I/O PC13 (i.e., pin connected to B1 User push-button) of another L476rg

I have need to output from a Nucleo L476rg to pin PC13 of another Nucleo L476rg, (i.e., to. the B1 USER push-button)Reason for input to this pin (which is connected to the blue USER push-button) is simply that all of the second L476rg's other pins ar...

GBumi.1 by Associate
  • 1342 Views
  • 1 replies
  • 0 kudos

Hello, i have to solve the task: Configure the MCU to operate with a system clock frequency of 72MHz. Make sure that the clock signal is derived from the external oscillator (HSE). Find a way to show the system clock frequency (SYSCLK) at an output pin.

This is my code so far.I solved the clock frequency of 72MHz with an excel sheet and imported the file which got created, so that is working. My HSE Speed is 8 Mhz.Now i dont get how to mirror the System Clock onto the MCO output pin.This is what i t...

DKunz.1 by Associate II
  • 2729 Views
  • 5 replies
  • 0 kudos

Resolved! GPS data collection using UART6 of STM32F411VEH6

Hello,I am using NEO M8U as GPS sensor in our custom board.GPS data is has to be collected using UART6 of MCU(STM32F411VEH6). Signal names in schematics as (MCU_GNSS_UART_TX and MCU_GNSS_UART_RX).Code has been attached . I am unable to receive data. ...

GBISW.1 by Associate II
  • 6274 Views
  • 7 replies
  • 0 kudos

STM32F4 I2C SDA & SCL rise time

Hi, I working with STM32F401RET6 64 pins Nucleo board with IAR.According to the datasheet DM00086815 Section 6.3.19 SDA and SCL rise time = 300ns.I open the project from “STM32Cube_FW_F4_V1.25.0�? STM32F410xx-Nucleo\Examples\I2C\I2C_TwoBoards_ComPoll...

0693W000006EojXQAS.jpg
gil23 by Associate III
  • 4176 Views
  • 6 replies
  • 1 kudos