User Activity

I'm currently using the dual-core STM32H745, and am trying to utilize DMA's on both cores to R/W to/from shared memory. DMA's are only successful on the M4 cores, and always yield a DMA Transfer Error. I haven't done anything to modify the initializa...
Hello,Looking over the STSpin implementation of the Clarke Park transforms and SVM has raised some questions about the derivation of the transform. Typically the the Clarke Transform takes the form of:퐼훼=퐼푎퐼훽=1√3(퐼푎+2퐼푏STSpin's implementation effecti...
Hi all,I'm attempting to run the simplest example code provided for the STM32H745XI dual core (M7 and M4 cores). I've configured my cube debugger as explained in the link below, and I'm having no success debugging or even starting the second core (M4...
Hello,We are using the STM32H745 dual core series, and have an image size that is nearing the single flash banks limit of 1MB. We won't be using the swap bank feature at any point. Will there be issues if the image overlaps the second bank?
Kudos from