STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Disable internal SMPS by Harware STM32H755IIT

Well I tried to read the documentation, but found only HW requirements to use SMPS. So is the SMPS required?Or can the SMPS just tie VDDSMPS, VLXSMPS, VFBSMPS and VSSSMPS to ground directly on PCB when no needs for that?

Kura by Associate II
  • 1707 Views
  • 1 replies
  • 0 kudos

Use basic DFSDM on STM32F12ZG

Hi,I am trying to record audio on a STM32F412 with an MP23DT05-A (digital MEMS microphone made by ST) using DSFDM.After basic configuration in CubeMX the project does not compile. The error is a missing function: undefined reference to `__HAL_RCC_D...

Resolved! Using SPI with STM32L4R9 Discovery Board

Unfortunately there isn't an example provided for SPI on the STM32L4R9 Disco board. I can tell from the User Manual that I need to set the quad SPDT switch on the board to the SPI configuration. If I understand table 20 in the User Manual, I need to ...

magene by Senior II
  • 1665 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F030K ADC injects voltage on pin

Hi, Can anybody help to point out why the pin voltage on adc input goes high as soon as i start the adc. When I connected a 10K resistor between AIN1 and GND (VDDA=VDD=3.3V), the voltage dropped to 1.6V. I tried HAL_ADC_START , Start with IT , DMA...

PVD (Programmable Voltage Detector) interrupt not working

Hello,I am using NUCLEO-STM32G071RB hardware. I configure to detect PVD (falling edge) but it looks like it doesn't detect any interrupt./** * @brief Configures the PVD resources. * @param None * @retval None */ void PVD_Config(void) { /*...

HBavi.1 by Associate III
  • 2548 Views
  • 3 replies
  • 0 kudos

Getting Started with the STM32L562E-DK Development Kit (2)

Hi,I'm trying to get familiar with the STM32L5 series of MCU's by loading and executing one of the example projects on the STM32L562E-DK Development Kit. The user manual for getting started with STM32L5, UM2656, says that there is an example project...

BMcMi.1 by Associate II
  • 1504 Views
  • 1 replies
  • 0 kudos