STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-F446RE - CAN Bus not initializing.

Hello!I have been trying to get the CAN system on this to work unsuccessfully for some time now, and in trying to debug the code have added some SWV ITM console printf's. In running the code, the HAL_CAN_Init, HAL_CAN_ConfigFilter, HAL_CAN_ActivateNo...

Aaronium by Associate III
  • 6781 Views
  • 7 replies
  • 0 kudos

Resolved! CAN interrupt is not called

Hello,I am trying to set up a CAN interrupt base communication system and it seems that IRQ handler is never called.Debugger goes through the CAN1_TX and then back to main function, so IRq is never called.USART output:[2020-12-08_21:19:01:191] A...

Kaveh by Associate III
  • 1964 Views
  • 1 replies
  • 0 kudos

Resolved! Issues with SPI comms between two STM32s

I'm trying out simple SPI comms between two STM32s. The TX is STM32F407 and the RX is STM32G070. The data that I seem to be receiving is different from what I'm sending. What am I missing here?For the RX, I've set the NSS to software. I've configured...

0693W000006Gw3KQAS.png 0693W000006Gw4RQAS.png

Trouble setting D2 clocks

I'm trying to set up the clock tree, and D1CKRDY becomes ready, but for some reason D2CKRDY does not. Here is the code:// Clock setup   RCC->CR |= RCC_CR_HSEBYP; // Set HSE as...

Neuromod by Associate II
  • 859 Views
  • 0 replies
  • 0 kudos

Changing data for DAC every 1 sec

Hello,I currently use the STM32G4 MCU Nucleo board (NUCLEO-G474RE) - I create an array of numbers (specifically - a sine wave at a certain frequency), which I transmit via the DMA, triggered by a timer (TIM2). Currently, the array is being transmitte...

YLivn.1 by Associate II
  • 2463 Views
  • 4 replies
  • 1 kudos

Resolved! STM32F042 CAN bus receive problem

Hello,I want to receive messages from CAN bus using STM32F042, but I have a problem with it because the interrupt is not working.I can send messages without any kind of problem, the problem is only with the receiving.I have set up the filter as it ca...

PDavi.4 by Associate II
  • 2357 Views
  • 2 replies
  • 0 kudos

Resolved! Disable internal SMPS by Harware STM32H755IIT

Well I tried to read the documentation, but found only HW requirements to use SMPS. So is the SMPS required?Or can the SMPS just tie VDDSMPS, VLXSMPS, VFBSMPS and VSSSMPS to ground directly on PCB when no needs for that?

Kura by Associate II
  • 1707 Views
  • 1 replies
  • 0 kudos

Use basic DFSDM on STM32F12ZG

Hi,I am trying to record audio on a STM32F412 with an MP23DT05-A (digital MEMS microphone made by ST) using DSFDM.After basic configuration in CubeMX the project does not compile. The error is a missing function: undefined reference to `__HAL_RCC_D...