STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't update GPIOx_MODER register value in STM32H753.

I work with STM32H753 through 3-rd side hardware (Algocraft WN-1 programmer) and have an access to the registers. I try to read/write GPIOJ pins. For this purpose I enabled GPIOJ clock by writing the AHB4 peripheral clock enable register (RCC_AHB4ENR...

LKuri.1 by Associate II
  • 997 Views
  • 2 replies
  • 0 kudos

2021 STM32 Wish List

Dear Community Members & STM32 fans,Peculiar year it has been, 2020 comes to its end. This is an opportunity to say "Thank you" because:you don't hesitate to bring help to othersyou help us improve our STM32 offeryou have confidence on ST Communityyo...

Resolved! AXI SRAM losing last few writes across reset

it seems that a write to AXI SRAM very shortly before a system reset (via AIRCR) gets lost. I wrote a very short block of code that simply reads a word from 0x24000000, increments it, writes it back, and resets the processor. I can see that the value...

CHead by Associate III
  • 7804 Views
  • 12 replies
  • 2 kudos

Bluetooth with STM32

Is there any part from STM which able to operates as bluetooth HID keyboard as well as bluetooth touchpad?

Bs.1 by Associate II
  • 662 Views
  • 0 replies
  • 0 kudos

Floating input pins under startup - is it really that bad?

Hi :) So I keep reading everywhere that leaving a CMOS input pin floating is bad because it is high impedance, can oscillate, etc. I understand and agree.But while a MCU is starting up (or when you're programming it) all its pin are in input state un...

SLasn.1 by Senior
  • 5588 Views
  • 7 replies
  • 0 kudos

Resolved! Running SPI receive in the background

Hi, I have a STM32F407 board that is running as a full duplex slave. it receives data from a Raspberry Pi configured as a SPI master. Is there a way to receive data from the RPi in a non-blocking mode? One way I could think of was to set the CSN line...

Difference in programing STM32L562 and STM32H735 MCU

Hello, In my project I need to have MCU that can handle lot's of data and be power efficient when I need to. In first, i was running STM32L562, but it looks like I will need tones more performance to complete many tasks in time.I use DMA alot, for se...

Linas L by Senior II
  • 1286 Views
  • 2 replies
  • 0 kudos

How to keep RTC ticking when wakeup enabled?

Is there a way to make the RTC continue keeping time while the wakeup timer is enabled? On my end, time freezes whenever the `cr.wute` bit is set.The RTC is listed as frozen in init mode, but It's not in init mode. It could be a shadow register issue...

DOCon.1 by Senior
  • 1360 Views
  • 2 replies
  • 0 kudos