I set up the VREFBUF (using CubeMx) to use the internal voltage reference, with a SCALE of 2.048V. When i probe the Vref pin i see a voltage of around 2.2-2.3V, it changes slightly after ever power reset. It is a custom board with a G061c8 micro. The...