STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! gpio let down 5 V pull-up

I use stm32f401's PB4 (NJTRST) pin. I attached 5 V pull-up resistor (5.1k) to PB4. While MCU is in reset mode the voltage on PB4 is 4.26 V. Only after starting the system, the voltage increases to 5 V. In my program I configure PB4 as input without p...

How to make NUCLEO-H745ZI-Q do anything?

I've been trying to make LED blink. GPIO PE1. So i wrote this code:HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_1);HAL_Delay(200);When i'm creating procject for this board it creates two procject for each core CM7 and CM4 each with it's main.c. I can debug eac...

KBile.1 by Associate II
  • 3163 Views
  • 6 replies
  • 0 kudos

Newbie question about PWM output accuracy

Hi, I'm testing various PWM scenarios and found that output frequency does not match with expected. I'm using formula Period = (PSC+1)*(ARR+1) / TmerClockFreq in seconds Period = 1000 * (PSC+1)*(ARR+1) / TmerClockFreq in milliseconds. The board is Nu...

SZony.1 by Associate II
  • 5465 Views
  • 10 replies
  • 0 kudos

GAM module of X-CUBE-AUDIO does not work with STM32L

I tried to use GAM module of X-CUBE-AUDIO. In the documentation, it says that it can be used with any STM32 which possess M4 core however when I try to use it with STM32L series one, the function of the module returns -6 which indicates wrong hardwar...

Oozzy.1 by Associate II
  • 1831 Views
  • 5 replies
  • 0 kudos

Setting Brown-Out Threshold in Option bits

Hi,for my application, I need to set my BOR threshold to about 2.5 V in my STM32L476RG. My understanding is that the preconfigured threshold is at level 4, which is 2.8 V (see RM0351 Rev 7, page 111).What is a good strategy for setting the BOR_LEV bi...

AHass.1 by Associate II
  • 2121 Views
  • 1 replies
  • 0 kudos

STM32L0C8T6 failed to communicate with M24C02 through IIC

STM32L0C8T6 failed to communicate with M24C02 through IIC,iic uses cubemx default configuration,The relevant code show as below:​#define ADDR_24LCxx_Write 0xA0#define ADDR_24LCxx_Read 0xA1#define IIC_BufferSize 256uint8_t IIC_WriteBuffer[IIC_BufferSi...

0693W000006HdlxQAC.png
*于.1 by Associate II
  • 1343 Views
  • 2 replies
  • 1 kudos

Resolved! Not sure to whom to address my question: Question about Virtual Com-Port-Driver 1.3.1.0 installed on WIN10. The manager states "STMicroelectronics Virtual COM Port (COM 6)". But my attached ext. divice, which I want to access only accepts port 4!?

How can I change the driver to port 4 or how can I install the driver additionally for port 4? *Edited by moderation: please don't mention your email address publicly on this forum*

MKnap.1 by Associate II
  • 1800 Views
  • 4 replies
  • 0 kudos

STM32F103 SPI Slave strategy

I use STM32F103C8T6 as SPI slave and want to send data on request by master.The master sends to the slave a byte, which has to be used to decide, what has to be doneor what data data has to be sent to the master, and a fill byte which is neededto shi...

DNeum.1 by Associate II
  • 3346 Views
  • 5 replies
  • 0 kudos