I'm using the stm32f030k6t6 microprocessor without the devkit, just the module, and I'm using cubeIDE (cubeMX V6.0.1) to generate a code to read a temperature from a sensor connected to PB0 (ADC_IN8). The problem is that when I start the adc (HAL_AD...