STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard Fault when dicrease core freq on F373

Hi, I'm using STM32F373 for my project. When I'm using core freq >=36MHz everything is fine. But I need to decrease core freq for power consumption. When I run project with 12/24MHz Hard Fault is occurred in 1-5 secconds. Times is randoms. (Of course...

AFili.1 by Associate
  • 1548 Views
  • 2 replies
  • 0 kudos

Updating firmware using raspberry pi

I have a custom board with SWO pins for STM32 firmware (but I don't have the RESET pin)I was planning to update my board remotely with ST-Link and raspberry piBut I found out too late that STM32CubeProgrammer does not support ARMI tried to use ST-Lin...

Does STM32 have registers to determine the restart type?

STM32L051C8, use standby mode; exit is equivalent to restart; whether there is a flag bit to determine the type of restart; for example, power-on restart, watchdog restart, low-power wake-up can be distinguished; whether it can distinguish the standb...

*于.1 by Associate II
  • 1431 Views
  • 5 replies
  • 0 kudos