STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G474 MCU port protection

Hi Folks,Greetings!At my end have a STM32G474 HRTIM output driving a MOSFET gate driver such as IR2110.In some weird cases encountered, when the MOSFET blows up, it takes away with it thegate driver as well.Not in all cases, but in some situations, I...

UART interrupt not working properly on STM32H753 MCU?

I am using STM32H753 MCU. I generated my code using STM32Cube. The UART is configured to work on interrupt, baud rate is 19200. I sent 'A' many time but most of the time I am receiving "C1" in hex instead of "41" ('A' in ASCII).When I analyzed the da...

Akash_k by Associate III
  • 1069 Views
  • 0 replies
  • 0 kudos

Write Backupcode from QSPi to SDRAM when flashing from IDE

My application is executed from flash and external SDRAM.I have a bootloader(seperat project) that saves the volatile SDRAM content on a QSPI.Normaly my application is applyed by a .hex file that is located on the SD-Card. So my bootloader can clearl...

Minti by Associate II
  • 686 Views
  • 0 replies
  • 0 kudos

STM32H753 ADC auto calibration not working properly?

I am using STM32H753 MCU. I am using ADC1 and ADC2 and calibrated the ADC offset using auto calibration function. But this function is not working properly. I am getting a difference of 50 counts on subsequent starts of my device. I checked this by g...

Akash_k by Associate III
  • 1232 Views
  • 1 replies
  • 0 kudos

Errors in STM32F446RE datasheet

Refer to https://www.st.com/resource/en/datasheet/stm32f446re.pdfIn section 3.23 on PDF page 32, it says:"The devices embed four universal synchronous/asynchronous receiver transmitters (USART1, USART2, USART3 and USART6) and four universal asynchron...

JArmi.1 by Associate II
  • 1117 Views
  • 1 replies
  • 0 kudos