User Activity

I am using CubeIDE 1.11.2 with a STM32F3DISCOVERY board and have created an IDE project via the integrated CubeMX GUI.I want to activate read protection via HAL_FLASHEx_OBProgram as well as the write protection for the FLASH area of my firmware (appl...
Hello,my question implies that there is no value for TS_CAL2 available for the STM32G070, although its reference manual RM0454 describes it on page 292 (14.9 Temperature sensor and internal reference voltage: Reading the temperature). Since there is ...
When starting the freshly installed STM32CubeIDE V1.0.1 on Windows7 none of the PDF documentation files are accessible (also no error message will be displayed), just nothing happens.When searching the installation directory there are some PDF files ...
Posted on February 13, 2018 at 13:16The current data sheet for the STM32F303CC (DocID023353 Rev13) shows on page 80 the characteristics of the LSI oscillator.Its frequency starts from min. 30kHz to typical 40 and max. 50 kHz (all at 3.3V in the max....
Posted on December 20, 2017 at 15:51I know of the STM32F303 line with 5MS/s (0.2us),the F378 with slower ADCs but 16-bitand some F4/F7 devices with also slower than the F303 ADCs.But which STM32 has the fastest ADC regarding the complete conversion ...