STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747: UART7 with DMA.

Hello!I have strange issue with DMA mode for UART7. I have callback for data transfer complete, but if i sending new data - i have broken data. If i added timeout - all data sending Ok.does anyone have any thoughts?

VLesc.2 by Associate II
  • 2195 Views
  • 4 replies
  • 0 kudos

Erase Flash in STM32H730ZB by flash word.

Hi,I want to implement custom bootloader in STM32H730ZB, It has 128KB of Flash and only one sector. If I want to load image using bootloader then, I need to erase particular portion of flash. Is there any support to erase flash by flash word? If I er...

BPanc.1 by Associate
  • 688 Views
  • 0 replies
  • 0 kudos

Resolved! How do you start DMA with interrupts? huart4.Instance->CR3 |= USART_CR3_DMAT; HAL_DMA_Start_IT(&hdma_uart4_tx,(uint32_t)msg, (uint32_t)&huart4.Instance->TDR,len); Works the first time, but if you change msg and len it repeats first case.

I need the callback, to clear the cb4.DMA_Active flag and update a pointer when it finishes. I cannot step through it because it starts sending data over and over as I step through it and does not call the callback. First time msg points to "12345678...

KiptonM by Lead
  • 1737 Views
  • 3 replies
  • 0 kudos

We are using STM32L476 in our application in which we have seen accidental change in RDP level when battery voltage drops below 0%. Is there any corner case we should take care?

In code, we do not have call for changing RDP but we have a logic to reset IWDG_STOP bit after wakeup from sleep mode. We are facing this option byte corruption problem when battery drops below 0%. (We do not have HW support for cutting off power for...

kpate.11 by Associate II
  • 4647 Views
  • 13 replies
  • 0 kudos