cancel
Showing results for 
Search instead for 
Did you mean: 

RM0440, Rev 4, STM32G4 Reference Manual - Section 13.6.1 information missing

Singh.Harjit
Senior II

Page 435, the explanation for Bits 28:24 ends with "(see )."

This is a real cliff hanger! ;^)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen GH
ST Employee

Hello @Singh.Harjit​ ,

I take your feedback into consideration and I will raise this internally.

Thank you.

Imen

Uwe Bonnes
Chief

Probably the reference should go to page 428 "Table 93. DMAMUX: assignment of synchronization inputs to resources". However this does not match with "Number of DMAMUX synchronization inputs 21"

Imen GH
ST Employee

Hello,

I confirm. it should say:(see Table 93. DMAMUX: assignment of synchronization inputs to resources).

I have already raised internally to correct the RM error in next release.

Regards