STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, after clicking "Register", the page returns 'No more seat available for this location" Do you plan additional workshop in this topic?

I'm using smaller MCUs (L4, F3, ...), but I'd like to learn running the code from external memory.Use case: not change the MCU to the bigger one, but add external memory e.g. via QSPI.I thought this workshop is good starting point.

What happens if CPU registers are stuck at fault.

For IEC60335-1 class B compliance, CPU registers should function well(Should not be stuck at faults). To test those faults we need to send/store some instructions to those registers. What if those registers are stuck at fault? I mean If it is stuck a...

Anitha by Associate III
  • 658 Views
  • 0 replies
  • 0 kudos

Resolved! Initial state of pins on STM32G0.

Hello. I have a circuit containing notably: (i) MCU pin PA2 connected to both a ULN2003 transistor-array input and a 10k pulldown resistor and (ii) the corresponding output of the ULN2003 is connected to a small beeper GND. In theory, this circuit is...

JLemi by Associate III
  • 2859 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L0 - GPIO Interrupt blocking RTC Interrupt

Hello,I have the RTC set for a 1 Hz interrupt. I have buttons, that when pressed, trigger a rising edge interrupt. The interrupts work fine except that when I call my button handling routine the RTC interrupts are blocked. They remain block until the...

RSoen.1 by Associate III
  • 2337 Views
  • 3 replies
  • 0 kudos

How to get an 8MHz sine wave HSE output on pin MCO1 (PA8) and should it be in phase with the original crystal signal?

I have been told i need to sync 2 STM32 MCU's together (on the same PCB) to stop an intermittent I2C bus failure between them. At the moment they are operating on separate 8Mhz crystals. I have used the following command to configure and output the 8...

Resolved! External interrupts on PC14 and PC15 of STM32F103C8T6.

Hello, guys.I need to improve one old project. There is no free pins on MCU left, except PC13-PC15 and I need three external interrupts. Code with initialization for making PC13-PC15 as inputs lower. I do not use LSE or RTC anyway.For PC13 all works ...

Antony1 by Associate II
  • 3157 Views
  • 4 replies
  • 0 kudos

TIM4 is a master, TIM3 is a slave. Given the same values I expected their respective CCx IRQ to fire at about the same time.

Set up TIM4 to generate a hsync pulse of 2us RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); TIM_Cmd(TIM4, DISABLE); TIM_TimeBaseInitTypeDef timerInitStructure; timerInitStructure.TIM_Prescaler = 0; timerInitStructure.TIM_CounterMode = TIM_...

0693W000007YzcbQAC.png 0693W000007YzbZQAS.png 0693W000007YzclQAC.png

Resolved! Build server vendors (CI/CD) for STM32?

I'm looking for any potential vendors where I could host a cloud VM for doing automated STM32 builds coupled with some infrastructure for managing releases? Any recommendations?

AVoel.1 by Associate III
  • 2684 Views
  • 3 replies
  • 0 kudos