User Activity

Hi everyone, Trying to create an eeprom API based on the AT24CM01 ASIC chip. I got the Byte write working no problem, however the IC is capable of doing sequential writes up to 256 bytes. The way I am doing this is setting the 'RELOAD' value within t...
Hey guys,Kinda pulling my hair out as to why the pull up resistor is not kicking in? I am expecting when the MCU boots up to see a nice high signal on PA4, but nothing. I am not sure what I am doing wrong. if I write a 0x01 into ODR it then pulls up,...
Hi everyone,I am trying to get the SAI1 periperhal configured in I2S Standard mode going on the STM32H753ZI. During my testing sessions I found that my master clock is so far off it doesnt make sense. Based on the figure 652 within the TRM, it shows ...
Hi everyone,I am having a hard time trying to get the max clock frequency out of the STM32H753ZIT6U.This is the revision V model and is capable of hitting 480MHz unlike its Y revision. This is my code to get to 480MHz:LL_PWR_ConfigSupply(LL_PWR_LDO_S...
Hi everyone,A new issue has occur and have no idea as to why the transmission would be sometimes corrupt. I try sending the word "Hello World" as a test, however sometimes I would receieve the word but sometimes I would receivbe garage values that va...
Kudos from