STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 I2C - is it possible for slave MCU device I2C interface to stop functioning while the rest of the I2C master MCU and attached devices carry on communicating happily?

I have an STM32F401 MCU acting as a master on its I2C1 port linked to a slave STM32F407 MCU, and a couple of DIO expanders (PCF8575). After a random period of between minutes and days the Master appears to stop updating the Slave MCU but continues to...

I2C wakeup sequence for ATSHA204A

The crypto chip ATSHA204A needs a >60us low pulse on the I2C SDA line to wakeup. After that pulse the SDA should be high for at least 2.5ms. How must the I2C be configured to create the described pulse? The attached pictures shows a transfer with ad...

LM35 Temperature sensor not able to read correct reading

Hi, i want to display temperature value of LM35 temperature sensor on oled using stm32f103. i selected adc channel . even i am able to read adc reading but it is not varying properly and even i am not able to read exact temperature reading. can anyo...

Lchal.1 by Associate III
  • 772 Views
  • 0 replies
  • 0 kudos

USART with DMA after stop2 mode not working.

Hi folks, I,m using STM32l4 MCU, I have configured USART3 with DMA1 with 1Mb/s baudrate. My concern is its worked fine if I don't put MCU in a Stop2 mode state. But if I put MCU in Stop2 mode state after waking up its not working. Here is the uart In...

ARehm by Associate III
  • 2625 Views
  • 3 replies
  • 0 kudos

STM32G071RB download pin?

I am using STM32G071RB. It is fine to connect only swdio, swclk, and gnd for program download. Is it necessary to connect the reset line?

CByou.1 by Associate
  • 1138 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L0 ADC register

I am using STM32L073.When using this ADC, the EOC of the flag ADC_ISR for which AD conversion has been completed does not change unless the EOCIE of ADC_IER is set.is it right.

HMura.6 by Associate II
  • 1263 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L475 - STOP2 multiple wake up modes

I have the STM32L475 working in STOP2 wake up as WFE based on the RTC. I would now like to add in an external interrupt source (WFI). There doesn't appear to be a way to use both a WFI and a WFE as wake up. The only way I could see would be to have a...

PVall by Associate II
  • 1161 Views
  • 2 replies
  • 0 kudos