STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L433CCU6 ADC problem (China PCBA)

Hi everyone, my project using STM32L433ccu6 MCU (PCBA from china). ADC value read out freeze 2048 (0x0800) , but in my prototype with component from Digikey or Arrow everything ok. And I try to replace MCU I bought from Digikey to PCBA board , It's w...

CBuek.1 by Associate II
  • 1134 Views
  • 2 replies
  • 0 kudos

STM32F407 Backup SRAM backup regulator needed ?

Hii would like to use the backup SRAM of the STM32F407 MCU to share boot flags between the bootloader and main firmware.The flag should be used to signal a "boot into bootloader" requested by the main firmware.To boot into the bootloader the main fir...

YWilk.1 by Associate II
  • 1242 Views
  • 2 replies
  • 0 kudos

STM32F302R8 - Not giving DAC output.

I am using the STM32F302R8 for motor control application. Need to do pulse-by-pulse current limiting.I have a BLDC drive board that has a comparator that can be used to give shutdown signal to the PWM. For this purpose, I need to give the comparator ...

VMuni.1 by Associate
  • 961 Views
  • 1 replies
  • 0 kudos

Can I use Python to program STM32?

I purchased a controller board from HiWonder, who use your STM32 MCU. I asked them if I can use python to program the STM32 but they do not know. Can I use python to program your microcontroller? Do I need to download specific software?

SMeza.1 by Associate
  • 16720 Views
  • 3 replies
  • 0 kudos

STM32H753XI Evaluation board - HAL_SPI_Receive() function return HAL_ERROR due to timeout for receiving data on SPI. What could be the problem?

Hi,I'm having a problem with SPI interface. I am using STM32H753XI Evaluation board. When I issue HAL_SPI_Receive function I get HAL_ERROR due to timeout for receiving data on SPI. What could be the problem?I attached my core dir.Thanks in advance.

RLevy.1 by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

Resolved! MDMA transfer not working STM32H7xx

Hello,I've been trying to transfer some data from AXI-SRAM to DTCM via MDMA but it seems not functional.The transfer occurs the flag of end of transfer is set yet the data that I have in my DTCM isn't the orignal one contained in the AXI-SRAM.Also im...

SGuic.1 by Associate II
  • 1239 Views
  • 1 replies
  • 0 kudos