STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Value of VREFINT_RDYF

Hi,I am reading value of SYSCFG_CFGR3_VREFINT_RDYF to be "1073741824". How do I interpret the value of VREFINT_RDYF from the value I am reading?

CDesh by Associate III
  • 1059 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H747 LPTIM4 PWM output in system STOP mode not working

Hi everyone, we have a problem using LPTIM4 PWM output on STM32H747I-DISCO when system enters STOP mode.In this project, I need two independent PWM outputs with fixed frequency to work, while system goes to STOP mode to save power. LPTIM1_OUT & LPTIM...

0693W000007Yz3HQAS.png
RChie.2 by Associate II
  • 2020 Views
  • 2 replies
  • 1 kudos

SPI1 stm32F103

Hi everyone,So, i would like to test SPI1 communication on my stm32F103, using just the clock and MOSI line by sending 0x55 data on MOSI line , but when i see the traces on logic analyzer, i'm getting a weird values !as seen in this capture picture, ...

0693W000007ZSegQAG.png
SIDRI.1 by Associate III
  • 944 Views
  • 0 replies
  • 0 kudos

STM32H7A3: SPI not working if SCK disabled

I am trying to emit data on SPI MOSI without enabling the corresponding SCK pin. This is useful for instance to control WS2812-type LEDs.​However when I use `HAL_SPI_Transmit_IT` to transfer 3 words, the IRQ Handler gets called 3 times (triggered by ...

AGebr.2 by Associate
  • 1933 Views
  • 2 replies
  • 0 kudos

ADC lines behavior when STM32 is not powered?

Hi!I'm using an ADC line of the STM32 MCU to read battery voltage that goes from 6.7V to 8.4V.The battery voltage is given to the MCU via a divider (by 4, so the maximum voltage given to the ADC line of the MCU will be 2.1V).I wanted to know, if ther...

YGehl.1 by Associate II
  • 1017 Views
  • 1 replies
  • 0 kudos

Touch Key in STM32L1

Hello, We are currently working on touch sensing in STM32L1V8XA Microcontroller Below are the queries :1) How to get started with cap sense touch key in STM32L1V8XA Microcontroller. Do we need to use STMTouch touch-sensing library https://www.st.com/...

JArot.1 by Associate
  • 638 Views
  • 0 replies
  • 0 kudos

Hello, I am a novice, I want to use rs232 to communicate with the computer in stm32f072cb,I want to enter 123 and post 456。I use PA9, PA10 is TX, RX

/** ****************************************************************************** * @file 01_Transmitter/main.c * @author MCD Application Team * @version V1.2.0 * @date 19-June-2015 * @brief This code example shows how to confi...

Hjing.1 by Associate
  • 2391 Views
  • 5 replies
  • 0 kudos