User Activity

Hi.I'm going to use in a design the SiP below, which contains a BlueNRG-355VC MCU inside.I have found the datasheet titled "BlueNRG-LP", and I was reading about the features of the GPIOs.When used as inputs, they can have internally connected pull-do...
Hi.For accelerometer LIS3DHTR, the output signals INT1 and INT2, pins 11 and 9, they are both push-pull (CMOS) outputs? or one of them, or both, have open-drain configuration?For my projects it is better that both INT1 and INT2 be CMOS outputs.Regard...
Hi.Currently we use SIM7000G and SIM7070G (GSM, NB-IoT, LTE-M, GNSS) modules from Simcom in our projects, using for authentication only a SIM holder with plastic chip, in the old way. We are starting to integrate the eSIM ICs on the boards, to use ho...
Hi.   I searched and did not found the part number(s) and datasheet(s) of ST's eSIM chip(s).  Could you help me please? I would like to employ an eSIM chip in a design.   Regards.
Hi.I was looking the datasheet of VNS3NV04P-E/VNS3NV04PTR-E that are SOIC-8 package, they have a Ilim of 3.5A and this is suitable for the project (2A is enough). The MOSFET would be driven by a 3.3V signal.I would like to know what happens if the po...
Kudos from