STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I am a novice, I want to use rs232 to communicate with the computer in stm32f072cb,I want to enter 123 and post 456。I use PA9, PA10 is TX, RX

/** ****************************************************************************** * @file 01_Transmitter/main.c * @author MCD Application Team * @version V1.2.0 * @date 19-June-2015 * @brief This code example shows how to confi...

Hjing.1 by Associate
  • 2395 Views
  • 5 replies
  • 0 kudos

Datasheat vs .stm32h745xx.h

I am trying to debug my USB and in the process I am going through all the registers defined in the datasheet vs stm32h745xx.h file and I see that in some cases the .h file has registers defined that is not in the datasheetGUSBCFG_CTXPKT : in .h but n...

LHoug.1 by Associate II
  • 863 Views
  • 1 replies
  • 0 kudos

Resolved! This specific CAN2 config crashes during HAL_CAN_Init(), why

Lets hope someone has a felicitously revelation, or a clue.I am using a custom board with a nice stm32f105rbtx, fed with external XTAL.Everything worked like a charm untill i configured the clock to be 72Mhz and readjusted the can parameters in CUBEM...

0693W000007ZNwVQAW.png 0693W000007ZNxsQAG.png 0693W000007ZNz5QAG.png 0693W000007ZO0DQAW.png
Javier1 by Principal
  • 1118 Views
  • 1 replies
  • 0 kudos

My potentiometer in a adc led counter doesnt work

Im trying to do an ADC led counter, but when i debug my program i see the live expression and i can watch the changes in the potentiometer, but D10,D9,D8 AND D7 are on but with 1.8v, and d5,d4,d3,d2 turn on with 3.3v, the main idea is that when i rot...

ALope.6 by Associate
  • 1555 Views
  • 1 replies
  • 0 kudos