STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using ITM printf on STM32H723 Nucleo board

Hi all,I'm tying to use the ITM printf on my STM32H723 Nucleo board in my Keil project without success. I configured the HAL with CubeMX and add the initialization for the SWD_Init(). I enabled tracing in Keil but I do not get any output. I checked:S...

JSchu.5 by Associate II
  • 12770 Views
  • 9 replies
  • 1 kudos

Why Nucleo F746ZG showing LD5 (Over current) on when running simple LED blink code? Also controller heating is more

Hello i am using Nucleo F746ZG board. When i run simple LED blink code with below code its not showing LD5 (Over current) on.#include "mbed.h"   // Blinking rate in milliseconds #define BLINKING_RATE 500ms int main() { // Initialise the digital pin...

Cjosh.1 by Associate II
  • 5880 Views
  • 11 replies
  • 0 kudos

STM32F469 IBIS Model

Hi,I am not able to download the IBIS model for STM32F469.I see a 404 error. Can someone please fix it.As first few STM32MCU ibis models show this error when we download.Regards,Ahmed

MAhma.1 by Associate
  • 1415 Views
  • 2 replies
  • 0 kudos

internal watchdog

Hey,im going to use the STM32h743 uCIn case the SW got stuck, is it possible to reset the program internally ?i would like "to save" implementation of External HW Watchdog. Moreover, do you have any recommendation for external HW circuit for Watchdo...

Pkats.1 by Associate II
  • 1827 Views
  • 2 replies
  • 0 kudos

STM32F0-Discovery Stop Current Consumption

hiI'm trying to write small application with wake up every 5min, I have tried to use Stop mode and looks like its working. I done some measurements and looks like current during Stop is around 8.8uA. Can you have a look if we can lower consumption?Ca...

KS by Associate
  • 916 Views
  • 0 replies
  • 0 kudos

LL_USART_TransmitData8 has problem in IAP.

I work on STM32H750VBT7 project using IAP. I cannot see right character (for example 0x30) output after calling LL_USART_TransmitData8. I do check TDR had got right content. The user program address is 0x8006000, I had changed VECT_TAB_OFFSET as 0x60...

LChan.5 by Associate II
  • 3466 Views
  • 7 replies
  • 0 kudos

How to enable Data Length Extension with BlueNRG-MS

BlueNRG-MS claims to support the Bluetooth Core Specification 4.2, which includes the data length extension. However, I don't find any pointers on how to enable it. For the BlueNRG-2, there appear to be special commands in the HCI LE API (see https:/...

ADusc.1 by Associate
  • 968 Views
  • 0 replies
  • 0 kudos

Video from USB camera to TouchGFX

I have a USB camera connected to a STMF746G Discovery board. I like to get the frames from the camera and show them in a TouchGFX application (e.g. using dynamic bitmaps). How do I get the camera frames? Is there any simple code example?

diewet by Associate
  • 570 Views
  • 0 replies
  • 0 kudos

Pin slew rate setting of STM32F746

Hello,GPIO port output has a speed register (GPIOx_OSPEEDR).When I use it for functions other than GPIO, can I set the slew rate with this register?If not, is there any other way to set the slew rate?Goto

Resolved! STM32F407 Uart Byte Received error(higher4bit)

Hi,​Using "STM32F4xx_DSP_StdPeriph_Lib_V1.8.0" to config STM32F407 Uart1 as following​///////////////////////////////////////////////////////////////////////////void USART1_Init(u32 baudrate){​ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef ...

0693W000008x1SVQAY.png 0693W000008x1R3QAI.png 0693W000008x1TEQAY.png
jhl14 by Associate II
  • 1095 Views
  • 1 replies
  • 0 kudos